Grundfos IE5 motors presented a success at the IFAT Eurasia 2017 in Istanbul

February 20, 2017

Grundfos IE5 motors presented a success at the IFAT Eurasia 2017 in Istanbul

As a pioneer in the pump industry, Grundfos were delighted to introduce one of the world’s most efficient motors, the new MGE with IE5 efficiency at the IFAT Eurasia in Istanbul, the Leading trade fair for environmental technologies.

When IFAT opened its doors in Istanbul, February 16-18th, Grundfos created an extraordinary customer experiences.  One amazing experience were the interactive product demos including the newly launched IE5, communicating the concept of Grundfos iSOLUTIONS as a holistic approach to system optimization.

Selecting a pump with the new IE5 motors will mean a 10% energy saving as well as up to a 25% reduction in payback time.

Not only are these motors capable of delivering an unprecedented level of performance, but their ground-breaking efficiency far exceed the forthcoming IE3 legislative standards, by actually meeting the strictest IE5 criteria – the highest energy efficiency level for electrical motors. New generation Grundfos MGE motors – from 0.25 kW to 11 kW – now qualify as capable of attaining this ‘super’ status.

The key to these MGE motors unparalleled performance lies in their state-of-the-art intelligent solutions as these adapt to the surrounding system and, coupled with the high-efficiency IE5 motor, drive down energy consumption.

With their integrated frequency converters, these motors combine the accumulated pump experience of Grundfos into their dedicated control software. This combination of pump and customizable software optimizes your system’s performance for any load point, delivering an unsurpassed reduction of energy consumption.  

All Grundfos MGE-motors in the range of 0.25 to 11 kW now qualify for the IE5 classification.