Mining industry

Overview

Grundfos offers mining companies a true partnership, with an organisational setup and expertise to meet your every requirement for a reliable pump solution for surface, open pit and underground mining. Grundfos pumps are built to last – even under the toughest working conditions.

Grundfos can supply to all processes and stages at the mine except initial transport and slurry pumps. Pumping solutions from Grundfos are available for all processes where liquids are to be pumped, even if they contain abrasives such as sand, clay particles, drill cuttings, and other potentially damaging objects, and also if the pH is very low, or if the media is aggressive, such as leachate solutions, or where the media is for cleaning and maintenance purposes.

In addition, Grundfos is a world leader supplying pumping solutions for water utilities, from raw water intake, to water treatment, wastewater transport and treatment, recycling and disposal. We ensure that the town built for your workers is fully equipped with utility pumps for all amenities.

With Grundfos as partner, we can always tailor a solution to an application. We offer great reliability with levels of continuous operation that ensure a high level of security for operations. Our tailored pumping solutions take account of requirements for special construction to cope with aggressive media, and utilise sensors and protection for pumps and motors that let you know there’s a problem before something goes wrong.

Our service agreements recognize the greater requirements for maintenance for mining applications. A partnership with Grundfos focuses on more than the pumping solution – we also focus on your business. Grundfos remains with you and your solution for the duration, offering commissioning agreements to ensure correct installation and service agreements with cover for all eventualities, from routine maintenance to spare parts and pump audits.


Grundfos - a responsible company
We demand from ourselves that our social and ethical behaviour must be in accordance with the international declarations for human rights and labour rights - and we will continuously make the same demands on our suppliers. Furthermore we will stimulate our customers to act in a socially and ethically responsible way.

Applications
Grundfos iSOLUTIONS

In mining applications, pumps do not operate in isolation, and the key to maximum efficiency and top performance is to optimise the whole system along with the pump.

Grundfos iSOLUTIONS is a holistic systems approach where advanced application-specific functionality and features makes it possible to obtain optimal performance, total energy efficiency, and ultimate reliability.

Grundfos iSOLUTIONS is all about getting the best solution for the task at hand.

Learn more on www.grundfos.com/isolutions

 

Downloads
Pump Handbook

Pump Handbook

[…] Grundfos has developed the Pump handbook, which in a simple manner deals with various considerations when dimensioning pumps and pump systems. We have elaborated a handbook for engineers and technicians who work with design and installation of pumps and pump systems, ...

Download PDF

17.7 MB/149 pages - Date:11/04

Pumps in water treatment

Pumps in water treatment

This book [...] focuses on water purification systems where the pump forms an essential part of the system. Therefore, rather than providing a complete picture of the field of water treatment, it covers water treatment with the pump as a central element.

Download PDF

2.9 MB/98 pages - Date: 01/02

Motor book

Motor book

This motor book will provide you with a wealth of information about electrical motors, how they work, what they can be used for, and so on. [...] As this is a Grundfos publication, it is only natural that we should pay special attention to motors used for pumps – although much of the information ...

Download PDF

16.5 MB/252 pages - Date:09/07

Mechanical shaft seals for pumps

Mechanical shaft seals for pumps

For most pumps a decisive element for the quality of the pump during its lifetime is a good and robust shaft seal. Grundfos has many years of experience with the development, …

Download PDF

7.2 MB/105 pages - Date: 07/09

Controls guide

Controls guide

The demands for controls increase and are often requested on pumps, when it comes to optimum operation, high reliability and monitoring of data. Therefore, Grundfos has developed the Controls Guide, which gives in a simple manner an overview …

Download PDF

5.6 MB/112 pages - Date: 01/12

Go further with high-quality pump solutions

Go further with high-quality pump ...

Backed by decades of experience of developing state-of-the-art pump solutions, we understand the challenges you face in the mining industry and design every one of our products accordingly to make sure they are tough enough to tear through some of the harshest environments on the planet.

Download PDF

1.3 MB/8 pages - Date: 04/14

Contact

We’d like to hear from you.

Please use the drop-down menu to find the Grundfos representative closest to you.

Telephone

(+2) 02 26 96 56 76

Fax

(+2) 02 26 96 56 77

Address

3 Gamaya Elhak Fi Alhaya st.,
Sheraton- Heliopolis,
Cairo 11361 - Egypt

Sales responsible for:

  • Egypt
  • Libya
  • Sudan