FAQ

Showing 21 to 30 of 88 results

The pump curve of a heating pump displays the feed rate on the x-axis and the delivery head on the y-axis. The pump curve shown in the graph is curved, dropping off from left to right.

Read more...

The dynamic total delivery head is also referred to as the

Read more...

The dry running alarm is triggered if the motor is running and the flow rate is less than 0.07 m³/h and the pressure is lower than the pressure set on the pressure switch.

Read more...

The number of switching cycles is unlimited, as the SQ/SQE is equipped with soft start integrated into the motor.

Read more...

A: Circulator pumps are generally used to circulate hot water. The temperature of the pumped medium is transferred to the pump, and it is normal for the pump's surface to be warm or even hot.

Read more...

Dry running of the pump can damage the mechanical seal and the motor. For this reason, the float switches should be arranged so that the fill level in the shaft does not fall below the minimum level required to operate the pump.

Read more...

Yes, that is possible. To do so, connect one phase and the neutral conductor.

Read more...

No, this is not possible, since the housing and the heads are designed to fit together.

Read more...

In order to increase the service life of both pump and motor, weather protection should always be provided.

Read more...

No, this is not permitted, as pump components that have come into contact with pumped media are not suitable for use in drinking water systems.

Read more...