FAQ

Showing 51 to 60 of 88 results

The pumped medium must be completely drained from the pump chambers.

Read more...

During frost periods, users often fail to ensure that the pumped medium is drained completely from the pump chambers.

Read more...

If the pump is operating too far to left on the curve, this simply means that the pump is delivering high pressure but at a flow rate that is low or non-existent. High pressure inside the pump stresses the impeller unit and thus increases pressure on the motor bearings.

Read more...

Unless specified to the contrary, the curves in the Grundfos documentation are specified for the density and viscosity of water at a temperature of 20°C (specific gravity = 1 and viscosity = 1).

Read more...

When a pump operates too far to the right on the curve, this simply means that the pump is delivering a flow rate greater than that for which it was designed. In other words:

Read more...

A cooling jacket, also referred to as a flow generator, ensures that there is always sufficient water flow across the motor surface in order to cool the motor.

Read more...

In a dry-running pump, the component that comes into contact with the medium (the wetted part) is separate from the motor.

Read more...

The pump's input power is the pump's power requirement under the present operating conditions.

Read more...

In this pump design, all rotating parts (shaft, rotor, impeller) are located within the can in the pumped medium. Cooling and lubrication is provided by the pumped medium.

Read more...