Heating system filling water requirement

VDI Guideline 2035 Part 1 has been in effect since 2005, and VDI Guideline 2035 Part 2 has been in effect since 2009. These guidelines represent recognised rules of the technology. Ongoing technical advances as well as efficiency improvements and energy optimisation mean that modern heat generators and heating pumps are designed with lower tolerances than they were in the past. These technical advances have led to increased demands placed on the medium pumped in the system, as defined by VDI 2035.