How do I install the underwater cable?

Before installing the underwater cable on the motor, you need to make sure that the cable plug is clean and dry. For ease of installation, the rubber parts of the cable plug should be coated with a non-conductive silicone paste. The screws that hold the cable in place should be tightened using the following tightening torques:

MS 4000: 2.0 Nm

MS 402: 2.0 Nm

MS 6000: 4.0-5.0 Nm

MMS 6000: 10 Nm

MMS 12000: 15 Nm