The pump is operating in "AutoAdapt" mode and is showing a constant power consumption of over 5 watts.

Remedy

The pump's power consumption changes as a function of the heating system's requirements. A power consumption of 5 watts is only displayed at the minimum speed, e.g. during night set-back.